I only want to display patterns changing at the maximum rate for a microscopic sensor application. Can i save the extra space for the DLPC300 + SDRAM and put what needs to be done in the main FPGA?
The DS seems not to give information on how to directly control the DLP3000 in sufficient detail.
I also didn't find out if i am able to achieve higher pattern rates by partially updating the DLP3000.
And still i am not sure how the patterns are updated. First the pattern is loaded into the DLP3000 memory, then it is transferred to the mirrors with a strobe/latch signal? So all the mirrors are updating at the same time?
There seem to be some restrictions on how the mirrors can be updated, some technology/lifetime issues, powerup / down, is this the reason for the DLPC3000?