This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP2010 TI Design now available

Other Parts Discussed in Thread: DLP2010, DLPC3435, DLPA2005

All,

The new TI design for the DLP2010 chipset comprising of ( .2 WVGA DMD, DLPC3435 controller and DLPA2005 PMIC/LED driver) is now available online. You can access the TI Design from:

http://www.ti.com/tool/tida-00325

Features of the TI Design include:

  • Reference design implemented on an EVM which includes a production ready optical engine with programmable LED driver ( 0 - 650 mA) for RGB LEDs
  • Includes standard HDMI input interface to connect any display device
  • Get started quickly with simple yet powerful USB-based GUI
  • This reference design is tested and implemented on a EVM available for purchase on ti.com and includes firmware, GUI and getting started guide

Regards

Anshul