This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DDP2000 general information



Hi, i want to use DLP projector circuit in my project of "DMD implementation of single pixel camera using compressed sensing". I have to project light on DMD in which some mirrors will be in '0' state and rest will be in '1' state. 

I want to know can it be accomplished with projector DMD and control board. If so, i want to know what is DDP 2000 function, what it does, can it be reprogrammed and how.  

If the datasheet is available then it is best but in other case some related information would be suffice.

  • Hi Saqib,


    The DDP 2000 is part of an OEM chipset and is not available as a catalog product. To achieve the control you are looking for, I would suggest looking into the LightCrafter 4500 or the CEL5500 Light Engine. It should be noted that the LightCrafter 4500 has a diamond pixel array, which may factor into your design.

    Please let us know if you have any additional questions!

    Thanks,

    Trevor