Dear All,
Can DLPC200 software operate at the Windows8.1 environment?
If possible we would like to operate the DLP5500 DMD from the Windows8.1 OS.
Can the current USB driver or dll files be used on the Windows8.1?
Best regards,
Rossinag,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Rossinag,
The DLLs and header files should be okay, i think using the dll and header file you should be able to build an application that can run on Windows 8.1.
I do see the driver installation procedure changed, it will now look for the digital signatures, i suggest you to refer to this link http://www.nextofwindows.com/how-to-install-an-un-signed-3rd-party-driver-in-windows-8/ about installing the DLPC200 driver.
Regards,
Sanjeev