Hello,
I saw the post in the below.
There is some issue in firmware version 2.0.
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/311314
Question)
- Is the issue applied to firmware version 1.1?
Because our system have produced with FWv1.1.
- Could you let me know the affected condition ?
Is that applied when using trigger mode 0?
or, pattern LUT load issue always happens when using I2C?
- When will you release firmware v3.0 ?
Best regards, RY