Dear Engineer:
I have a problem about how to use the API_DisplayStaticImage on the DLP Lightcrafter (DM365) Platform.
The function prototype is as follows:
typedef ErrorCode_t (API_DataFunc_t)(void *Param, uint8 *Data, uint32 Size);
ErrorCode_t API_DisplayStaticImage(API_DataFunc_t *GetData, void *DataParam);
The functions mentioned above are in the file named LCR_API.h
Could you tell me the relationship among the parameters. And how to use the API_DisplayStaticImage function .
Thank you for your time!
Haitao Deng