Hi,
I have questions about the DMD LVDS interface for DLP6500 chip. This is LVDS. It consists of clk, SCTRL and DATA. What kind of a signal SCTRL? Where should I set to "0" and where should set to "1"?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have questions about the DMD LVDS interface for DLP6500 chip. This is LVDS. It consists of clk, SCTRL and DATA. What kind of a signal SCTRL? Where should I set to "0" and where should set to "1"?
Thanks.
Hello Sanjeev,
Hello Eric.
What do you mean impossible?The projector uses the chip 4422, and it's not DLPC900. I believe that if I know how to control the chip, it is possible..
If the information is closed, so you can write about it.
I'll tell you why this is necessary.
1 I do not have RGB image. There are only 2 colors. Green and yellow. And I consider it one color.
2. The frequency of change pictures must be a multiple of 8 or 16kHz. Otherwise, a very large energy losses occur.
I think (do not know) that DLPC900 can not perform it. I need to try it without DLPC900.. And I have no DLPC900.
Regards,
Kuch
Hello Kuch,
Thank you for explaining your situation. Please understand, Sanjeev simply stated it is not possible because TI does not provide a way to drive the DLP6500 without the DLPC900. I added that it is a requirement from TI's point of view for reliable functionality and operation.
If we determine a solution using the DLPC900 we will let you know.
Regards,
Eric
Hello Eric,
1. The document DLPS053 -OCTOBER 2014 (DLP6500) p.11 written "VCCI Supply voltage for LVDS receivers 3.3V".
2. The document DLPS037 -OCTOBER 2014 (DLPC900) p.4 written "1.8-V LVDS (DMD interface)".
Do I need converters for connection of these chips?
Regards,
Kuch
Hello Kuch,
You'll find that this information, including information on Block Operations (which work slightly differently than on the DLPC410), are documented in the DLPC900 Programmer's Guide.
Best regards,
Trevor
Hello , Trevor
I've been playing a copper laser images. His pulse frequency of 8-16 kHz.
I want to synchronize the pulse rate and frame pictures. If this is not done then we have great power loss.
So I want from my device control chip dlp6500.
Therefore, I'm interested in the interface signals dlp6500. And I was particularly interested in block mode.
And I would be very grateful for any information on this subject.
Best regards,
Kuch
Hello Kuch,
Synchronization can be achieved with the DLP6500 through the DLPC900. If you trigger the frame pictures off of the pulse of the copper laser, (while in block mode for added speed), you should be able to achieve the effect you are looking for. For more information, see section 4.2.1 Trigger Commands in the DLPC900 Programmer's Guide.
Best regards,
Trevor