Other Parts Discussed in Thread: TFP401A
Hi,
I have some questions on fringes projection by DLP3000 and DLPC300.
I want to project the gray scale fringes and signal by VGA port and
I hope the circuit will be easy, so i just want to use the DLPC300 become the bridge between the computer and DMD.
Is it possible use VGA RGB signals and sync ports to drive the chip via parallel RGB ports?
Is it necessary using I2C signal to control the DLPC300?
Thank you.