Hello All,
I am currently having difficulties with connecting to my DLP device to my windows 7 Professional 64-bit computer.
Its current status in device manager is:
*in Device Manager: Network Adapters --> USB Ethernet/RNDIS Gadget#5 Appears.
*in View Network Connections: Local Area Connection 7, unidentified network, shared, USB ethernet/RDNIS Gadget#5 Appears.
*In the DLP LightCrafter Control Software-5.0.0: there is a Connect button which I click, but does nothing.
*The device's current IP address can be pinged.
*Upon turning on the DLP device, the device does show its ability to switch through all the light pattern (fine checker board, etc)
What I have tried:
*I have tried to restart the computer with the device's USB disconnected.
*I have tried uninstalling the driver and reinstalling
*I have tried several different static IP address within the same default gateway
*I have tried turning the DLP device on and off then hitting the Connect button within the GUI
*I have tried disabling the Local Area Connection icon of the RNDIS Gadget #5
Please Help.
Thank you.