Hello there,
I am directing a laser beam onto my DLP7000, and trying to project an image of the DMD onto a screen/sample. The beam goes directly to the DMD without any expansion, and I'm getting diffraction patterns as described by others in various posts. I understand that if using the DMD for imaging, this shouldn't be a problem as a projection lens can collect the diffraction orders and form an image.
However, I am a little confused if I want to image from infinity. I looked at an earlier reply that says:
you may want to use a lens that makes all the orders parallel (i.e. collimated space) then use a final lens to reimage them from "infinity". This is equivalent to cutting a lens in half and separating the two halves by whatever distance you need.
Referring to an illustration I found:
Does this mean then that:
1. adding a single lens 1f from the diffraction plane above will collimate the orders
2. then placing a second lens afterwards forms an image of the DMD 1f away from this lens?
So my setup would then use 3 lens total?
Sorry for the confusion regarding basic optics, thank you again!