How do I set up triggering of my camera with my CCD. I have the DLP EVM.
Thanks so much for your help!
Christine
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How do I set up triggering of my camera with my CCD. I have the DLP EVM.
Thanks so much for your help!
Christine
Great! An excellent resource for learning about triggering on the LightCrafter (also sometimes called the LightCrafter3000), is the LightCrafter User's Guide: http://www.ti.com/lit/dlpu006
Check out section 2.6, I think that should answer some of your questions.
I'm going to move this thread to the LightCrafter specific forum, as it will be a little more specifically geared toward additional questions, if you have any.
Best regards,
Trevor
Thanks this is very helpful.
I have a special camera I would like to use. What is the output from the dlp?
Best,
Christine