This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How can I get rid of the logo of TI in the LightCrafter4500.

Other Parts Discussed in Thread: DLP4500NIR

I'm making a try to use the LightCrafter4500 controling the DLP4500NIR.I have made many attempts to download a pattern with color half black and white,but there is no phenomenon on the DLP4500NIR,just the logo of your.How can I get rid  of it?Or How can I  make true my detemination?

Thanks!

  • Hello James,

    We have provided you information via private email.

    For the Forum shake, here is something you should do - 

    There is a .INI file that comes with the GUI software.

    Please change below parameter 

    from 

    DATAPATH.SPLASHATSTARTUPENABLE                               0x01       ; <1> 

    to

    DATAPATH.SPLASHATSTARTUPENABLE                               0x00       ; <0> 

    Rebuild the firmware binary with this .INI file.

    This should bring up the system without logo displayed.

    Regards,
    Sanjeev