Hi to all,
Currently I am part of a team doing research on successfully running a point cloud stitching algorithm with the DLP4500 Lightcrafter and a Point Grey FLEA 3 camera. In order to get acquainted with the system the team has followed the TIDA-00254: Accurate Point Cloud Generation for 3D Machine Vision Applications using DLP® Technology and Industrial Camera User's Guide and have run into an issue. On page 69 step 6 we are supposed to properly compile the open project and should work flawlessly, yet we are currently getting this error:
The process "C:\Qt\Tools\mingw491_32\bin\mingw32-make.exe" exited with code 2.
Error while building/deploying project 3D_Scanner_LCr4500_PGcam (kit: Desktop Qt 5.4.1 MinGW 32bit)
When executing step "Make"
The system information for my system is the following:
Windows 8.1 64-bit
Qt Creator 3.3.2 based on Qt 5.4.1(MSVC 2010, 32-bit)
If anymore specs or info is needed I would be more than welcome to share. Thank you for any help/direction.