Hi All,
we are developing an active vision SWIR system (Short Wavelength Infra-Red) with an illuminator at 1550nm that projects structured light (dotted matrix or something like). The area that we have to enlighten is about of 10 meter x 10 meter; the maximum distance between illuminator and the area is about 14 meter.
Is it possibile to create such structured light for our application or area/distance above mentioned is too big for DLP technology?
If it is possible, please can you suggest your best solution and evaluating kit?
Thanks in advace for your support,
Savino