Hi,
i just started working with a lightcrafter 6500 evaluation module. Through the GUI the device works fine, but i need to be able to develop my own software controlling basic functions of the device. I understand i should refer to the dlpc900 programmer's guide (www.ti.com/.../dlpu018a.pdf). I quite understood the logic of the write/read commands, but i never worked with HIDs, and any possible help would be appreciated.
Could someone please upload a simple code with a read and a write example (like the two reported in sections 2.2 and 2.3 in the guide) for the usb interface?
At the moment i am trying to do it with python and the pywinusb module, but an example code in any kind of language would be a great help.
Thanks for your help
Paolo