This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is DMD chip 1280-6038B compatible with 1280-6439B?



Hi,

Is DMD chip 1280-6038B compatible with 1280-6439B? Note the 8 in the former and 9 in the latter.

Many thanks.