This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

The DLPDLCR2010EVM will not start

Other Parts Discussed in Thread: DLPC3430, DLPC3435

I have downloaded and installed the DLP LightCrafter Display 2010 EVM software and connected the DLPDLCR2010EVM as pr instructions.

In the Information window I can see that the connection is established and I can see when I switch the unit ON, but the projector does not start. When I click on "GET" I can see that some fields are being updated, but not all.

This is what I get:

DMD: Empty

Controller: DCPC3430

PMIC/LED Driver: Empty

EVM software: 0.0.0

Firmware: 0.0.0

This software: 2.0

There are no error indications.

To me it looks like the DMD and PMIC/LED Drive are lacking software. Please advice what I should do!

Grateful thanks in anticipation.

Best

Olav Sandnes

olav.sandnes@kverve.org

+47 900 26 277