This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using DLP with a laser source-- I want to measure the location of the contact point and associated angles of attack when a cue tip hits the cue ball

As part of a high school senior project I  am trying to measure the contact point and angle when a cue tip makes contact with a cue ball.

My thought is to use a range-finder type laser and scan the expected surface area where the contact is made

Will need two such devices to get the plane of the cue tip and the location of contact with the cue ball.

Questions:

1) Can I use a TI optical mirror device with a laser at all

2) What is the time it takes to turn a mirror on or off

3) Is the mirror's position binary or can it be more finely controlled?

Would appreciate some answers that then give me a starting point for further specifying my requirement


Jozef sliwkowski

Edgartown, MA

302-500-2019

jozef_sliwkowski@verizon.net