Everything was working great this past week. But then when we tried to turn on the DLP the light flashed but it did not turn on. It appeared at there was something wrong with the power. We have had a lot of trouble with this component in the past due to the fragility of the connector and stress on it. So, we then made a new connector for power at J11. We noticed a bit of dark liquid on MSP430F2232. Also, a bit on the trigger Pin 4. We are sending a 3.3TTL output trigger to a camera but just with Pins 1 and 3.
I'm not sure when this problem started (ie before or after the connector at J11). Any ideas of what is going on?
Thanks so much for your help!
Christine