This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Loading a BMP image into the LightCrafter 4500

Other Parts Discussed in Thread: DLPC350

Hi - 


I just received the LightCrafter 4500 and installed the GUI.   I'd like to display a 912 x 1140 BMP image (dot-to-dot), by loading it into flash memory, pattern sequence mode.


According to the user guide, section 3.6, page 35 (bottom)...

To download the images into flash, a series of 24-bit images must be added to the firmware file using the
Add Images to Firmware subtab with the following steps:
1. Select the Image / Firmware tab and the Add Images to Firmware subtab.
2. Select a firmware file by clicking the Browse button next to "Firmware File."

I hit the "browse" button to select a firmware file.... however I have no idea where the default firmware file is located.... or its file name and extension.


Can anyone help?   Thank you.