I would like to drive a series of 8-bit monochrome images via the RGB interface of the DLP6500. I've considered treating the RGB interface as a way to send three images with one VSYNC pulse but is it possible to send data on only one color channel - say green - and increase the the VSYNC pulse 3x? In other words, can I send data on the green channel at 180Hz vs sending three images on the RGB bus at 60Hz?
Kind regards,
Tim