This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Trigger Out on ALP 4.1 HS

Other Parts Discussed in Thread: ALP

Dear,

We are using the 0.7" XGA DMD board from DLi.

We need to trigger both a video recorder and a flash lamp from the board.

There is apparently a single PIN connector for output trigger (n°8 on multipurpose connector J6).

Is there a way to get two triggers signals from the ALP 4.1 HS so that we could trigger both the recvorder and the flash?

With best regards,

Remi