If I want to control a DLP7000 DMD, what is the minimum I need to use?
This is for a science project about building a color swept volume volumetric display with 3 such DMDs (for red, green and blue). The cost of the DMD chipsets is under my budget but making them work together is not well documented. Getting 3 "Discovery 4100" ready kits which are easy to control I think will be extremely expensive, plus is out of stock and final seller's site is not in english.
I already have 3 DLP7000 DMDs and remaining budget of $2000. I need to control these 3 DMDs at 1900 Hz greyscale. What will you suggest me to use to control these DMDs, if there is anything at this price range?