On sheet 16 of the DLP4500EVM schematic, there are pull-up resistors on the four 12C pins (J3, J4, M2 and M3). When using the DLPC350 on my own board design, would these resistors be necessary if I am not using these ports?
On sheet 17 of the schematic, there are three pull-up resistors on reserved pins D1, C1 and D2. Are these resistors required if not using the associated test points in my design? On the same sheet, if I will not be using the UART0 port, should I place resistors on the unused inputs (pins L20 and L21)?