I need to get a spatial light modulator to adjust light intensity in addition to "on" and "off " of a NIR light source (830 nm, 1W). I think that I need to buy DLP4500NIR MDM and DLPC350 controller. I would like to know if the controller can be used to adjust the intensity of a monochromatic light source. Also since there is a built-in LED driver, is there a specific light source that we need to use?
Thanks,