I am using the DLP Light Crafter 6500 EVM and controlling it with the provided GUI. Unfortunately, since a virus update from may 11, Symantec Endpoint Protection blocks some functionalities of the GUI: When I choose the Pattern On-The-Fly Mode and then try to load an image, the GUI gets blocked by the anti-virus software before the opening dialog would appear normally (the detector says: Trojan/ Virus: SONAR.SuspBeh!gen604). Is it an error of the anti-virus software or could there be an update of the GUI which will solve the issue?
Thanks for your help and best wishes,
Stefan