This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DLP LightCrafter 9000 EVM - FPGA source code



Hi,

One question about DLP LightCrafter 9000 devkit. To verify if it is possible to make our own devkit based on DLPC9000 driver, I would like to have access to the source code of the FPGA Altera Cyclone V present on the DLP LightCrafter 9000 EVM.

Is it possible to provide me with it?

Best Regards, Yannick

  • Hello Yannick,

    The binary image for the LightCrafter 9000 EVM FPGA is available in the LightCrafter9000 Firmware and Software bundle. We have not released the source code for the FPGA. Would your application require a change to the FPGA source code?

    Best regards,
    Trevor
  • Hello Trevor,

    Yes, we have to modify the code of the FPGA in order to add interfaces and functionality like Ethernet port, memories and monitoring of the board (voltage, temperature, etc...). So we need the source code of it to be able to interface the DLPC9000 chips and to integrate more features in the FPGA.

    Best Regards,

    Yannick

  • Hi Yannick,

    Unfortunately, we are unable to release the source code for the FPGA right now from a supportability standpoint.

    I have sent along an E2E friend request so I can put you in contact with someone who can talk to you about possible paths forward. Just accept this, and I will be in touch.

    Best regards,
    Trevor