Okay, I think in my previous thread I was confused from the difference between "frame" and "pattern".
I want to project as fast as possible for a special project. Both refresh rate and "frame" rate.
If I understood the manual correctly, the maximum speed for streaming "videos" is 1440 Hz for 1 bit "frames"?
The settings in the GUI program is under the "HDMI" menu so I'm assuming that the "frames" are going to be sent via the mini HDMI cable?
But here the frame rate is set to "60" and "pattern" rate is set to 1440. And its 1 bit mode.
How can I understand this? it is confusing.
Can anyone explain me this, how frame relates to "pattern" and whether I can send 1440 frames/patterns each second to the Lightcrafter and if yes how, without me having to buy one first and try it?