I'm looking to purchase a DMD and controller for use in an atomic physics experiment. At the moment, I'm considering the DLP LightCrafter Evaluation Module (taking out the LED) or the DLP LightCrafter 6500. I have two questions that I wasn't able to answer very well by just browsing the website. I would appreciate any input you have on the questions below. Thanks!
1) Is there a maximum power with which I can illuminate the DMD?
2) How easy is it to "upgrade" from one DMD and controller to another? If I purchase the DLP LightCrafter Evaluation Module to test out my application but then later realize I need something with a higher resolution (such as the DLP LightCrafter 6500), is the computer software the same? Can I just replace one device with the other and use the same programming or do I need to start everything over from scratch?