Document file name: dlpu018a_DLPC900 Programmer's Guide (Rev. A).pdf
In the DLPC900 Programmer's Guide (Rev. A) I found two identical READ commands for I2C. Chapter "1.5.1 Read Error Code" states, that 0x32 is the command byte to use if an error code must be retrieved. However, chapter "2.4 Start Address", which refers to DLPC firmware programming, denotes exactly the same command byte in order to read flash start addresses. This isn't the case for the USB command counterpart which fortifies my opinion, that all DLPC command identifiers shall be unique. An error in the documentation?
Regards,
Robert