Hello Pedro, I bought EVM3010 (which has the PT3 720P DISPLAY ENGINE from eProtech--which looks similar to what you discussed above), and want to do put a fish-eye lens. I took off the focusing module from the assembly (shown below), and was surprised to discover that the light downstream the DMD is NOT collimated, because the image gets larger (rather quickly) the further I move a piece of paper from the module. I would like a collimated light post DMD. Do you think I should try removing the fish-eye lense from the optical module?
w/ regards,
Henry