Hello together
I am trying to connect to a DPP6401F via the I2C Bus.
When I am connected to the bus, I get only the following adresses.
0x1A
0x50
0x51
0x52
0x53
Can someone, gibe me some information about the adresses?
In the description I have for the interface it stands that the addreses are 0x34 or 0x35.
I am using a microcontroller which is connected to the I2C bus of a P1-Demo Board from anhuaoe.com.
I hope someone can help me and give me some more information.
Kind regards
J.Bargsten