This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Optical components needed for illuminating DLP Lightcrafer DMD chip with and an external Laser source



Hello 

 

I am a graduate student and I would like to use DLP Lightcrafter in a confocal microscopy project. I have successfully dissemble light engine of one DLP chips and used an external  523 nm green laser source to illuminate the DMD chip.I used a beam expander after laser to make sure the whole surface of the DMD chip was illuminated. I have not used a beam shaper so my illumination is not uniform. I just put the DMD chip with 24 degrees respect to microscope optical axis and in the image plane of the microscope. Now I can see the patterns of the DMD on the objective(40x NA=0.55) focal plane but I was losing lots of mirrors, diffraction was too much and the quality was not good.

 

 I have seen some papers in which the DMD chip was used in microscopy research however optical setup were not well described. I also saw some useful discussions about what were optical components inside DLP lightcrafter and DLP 4500 which gave me some idea about the design.

https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/850/t/162664 

https://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/278008

 

However there are some question on my mind regarding this issue.  My questions are followings:

 

1. Was any TIR prism used in DLP lightcrafter light engine (I could see that a TIR prism was used in DLP 4500 light engine but I could npt see that in DLP Lightcrafter light engine)? Is using a TIR prism necessary?

 

2. What is the functionality of the lens just after the tilted mirror and right in front of the DMD 3000 chip? Is it a condenser?(In DLP 4500 light engine there was not any lens in front of the DMD chip and there was a TIR prism).

 

3. In both light engine micro lenses were used so I am thing of a using a micro lens for that purpose. Is this Thorlabs lens for this application? https://www.thorlabs.com/newgrouppage9.cfm?objectgroup_id=2861 or 

 

4.Should I use a condenser lens just in front of the DMD?

 

I am sorry for asking too many questions. I would appreciate your kind reply.

 Thank you very much in advance.

Vahid.

  • Hi Vahid,

    We have a similar post about the LightCrafter light engine to the one you found for the LightCrafter4500. I included a link below. Let us know if this thread clears up some of your questions.

    e2e.ti.com/.../162664

    Thanks,
    Clinton
  • Hi Vahid,

    I believe you may have already seen the link I included above. However, your link to this post is broken. We'll be taking a look into your additional questions. Please allow a couple days for feedback.

    Thanks,
    Clinton
  • Hi Clinton,

    Thank you very much for your reply. I have seen that post related to DLP lightcrafter Light engine components and it was so helpful. As I mentioned in my questions in that post for DLP LightCrafter I could not see any TIR prism and I did not know the function of the lens in front of the DMD chip. MOreover, I started to work on the setup if there is any improvement I will post here maybe it would be useful for other members. I am also looking forward to hearing from you.

    Than you,
    Vahid.