This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AC-DC adapter for DLP Lightcrafter 4500 not available currently.

The recommended adapter 62-1186-ND  (12V 84W, Barrel Plug output, 2.5mm I.D. x 5.5mm O.D. x 9.5mm)  is currently available neither at digikey nor mouser. Any recommendation on where else it might be available?

The maximum amperage for the DLP Lightcrafter 4500 is given as 7A at 12 V. I am not planning to use any panda board currently. Would a 12 V, 60 W power supply suffice is such as case?