This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some questions about pico-projector module with optical engine

Other Parts Discussed in Thread: DLP3010

Hello,

   We demands the pico projection module have following performance.
   Resolution:720p (If impossible,480p )
   Power Consumption:1W@25 lm,3W@50 lm
   Frame Rate:support to 120Hz

  We have already contact many manufacturer,but they don't have such product to sell.(most module only support to 60Hz and I can't find any pico-module with 720p based on DLP3010).

They recommended Lightcrafter module to me,I know the module support to 120 Hz but the size is too large  and including FPGA board.We need pico-projector module used in product but not development board.

We have following Questions:

1.Can you recommended manufacturer can sell pico-projector module meet our requirement?

2.If can't meet all demands,We have not found pico projector module with 720p resolution and low power consumption,can you recommended manufacturer to me?(even only support to 60Hz)

3. In order to achieve 120Hz whether we must use FPGA?may be DLPC is not enough?

4.If we bought ordinary module support to 60Hz,and we control the module with external FPGA.Can we realized projection with 120Hz?

Thank you!