Dear reader,
I'm using a DLP Discovery 4100 kit to generate static and dynamic light potentials. The experiment requires the sequence to be triggered at a given time and stopped on the end image. This rules out the software trigger mode currently available as this waits for a key press and the runs the sequence indefinitely.
Using the hardware trigger mode, which requires a trigger to change frames in the sequence, I found that it only faithfully reproduced the sequence if the trigger (on/off) pulses were at least 200ms. This was a little disappointing!
Ideally there would be a mode where I can send a single trigger, which then goes through the sequence of images once at a given frame-rate, ending on the final image. Is there a way for me to achieve this or at least improve the rate at which I can trigger in hardware mode?
Also the maximum number of images I can hold in hardware trigger mode is only 20 before the RAM fills up. Much larger sequences can be loaded but they cannot be externally triggered for a single run through. Any suggestions on extending the capacity or triggering a single run?
Thank you for any information you can provide,
Harry