Hi,
My customer is using the DLPC200 and DLP5500.
My customer uses a LVDS(200MHz) of the interface of DLPC200 and DLP5500.
However, EMI due to LVDS has come out strongly.
※ PCB layout complies with the DLP5500 data sheet (DLPS014E).
【Question】
1. Do setting is possible to drop the LVDS drive capacity at DLPC200?
2. Is there an effective way as EMI countermeasure?
Best Regards,
hamada