This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

So how to stream frames at 2880 Hz/fps?

Other Parts Discussed in Thread: TFP401, DLPC350

The manual says Lightcrafter 4500 can stream at 2880 Hz refresh rate and fps in 1 bit mode and "external mode".

But I don't see any ports that are fast enough to send over 200 Mbytes of data each second.

Am I correct to assume it is done via the HDMI port and every 24 frames have to be grouped into 1 24 bit frame before sending via HDMI and the Lightcrafter board will decode it back into individual 24 1 bit frames?