I am thinking about using LCr 4500 EVM as active illumination for imaging. At this point, only thing I want LCr 4500 to do is lighting my target with a sequence of specified colors. And imaging will be done with a high-speed camera with external trigger.
Now my questions are:
1. Is this possible with LCR 4500? I thought about simply using video mode with pre-defined images but I realized video mode is displaying images with 60Hz. This might cause flickering problem with the high-speed camera. And then I am not sure structured light mode has color option in GUI application.
2. If this is possible, how can I do it with GUI or programmatically (preferred method)?
3. Is there any recommended procedure for color calibration with LCr 4500?