This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to display all images from Flash memory of DLP4500 after introducing delay between successive images

Other Parts Discussed in Thread: DLP4500, DLPC350

Hello,

I have uploaded a number of 24-bit BMP images onto the Flash memory of DLPC350 on DLP4500 EVM.

I want to display all of these images on the DLP with some delay introduced in between the successive images.

1) Is there a way that this can be executed with an external trigger? How do you access the addresses of the images and display them according after introducing a fixed delay?

2) If this cannot be done with the use of flash memory as an input source, what other options can serve the purpose??

Thanks,

Pracheetee