Hello,
I am following TI’s user guide TIDA-00254 and other documents for 3D scanning. Only different setup from the documentation is that I am using Grasshopper3 Color camera but this seems to be not a problem because trigger is already working fine with the software (3D_Scanner_LCr4500_PGcam.exe) TI provided.
My problem is that LCr 4500 does not provide any illumination for menu item 4 (Calibration camera), 5 (Calibration system), and 6 (Perform scan) whatever I do while blinking green LED on the device.
As the documentation recommended, I have done menu #1 (Generate camera calibration board) and #2 (Prepare DLP LightCrafter 4500). But I have noticed the problem when menu #4 is selected. The program said "Projecting white pattern to illuminate calibration board" but nothing came out of the projector. This symptom is same for menu #5.
I thought I did something wrong for menu #2 (Prepare DLP LightCrafter 4500) but whenever I selected the menu, it finished the setup without any error message saying "Projector prepared" Actually, projector displayed a pattern at the end of the setup.
I tried GUI application and found no problem with operating the device with the software. Of course, the problem is not due to opened GUI application. Any helpful advise would be appreciated.