Hi all,
I purchased a B2B extension flex cable from keynote photonics and have implemented it. However, now the dmd does not seem to respond to any pattern I upload to it. I am using the bare (light engine removed) dmd with a 660nm laser source and when I load an image sequence or preset image onto it I see no change in the beam. My question then is:
Is there any way to diagnose if the DMD itself is connected to the chipset through the GUI?
Thanks, Sam