I've been working on talking to a DLPC350 over I2C and today came across the forum. Specifically, I can't write LUT entries via the mailbox over I2C. I found the threads:
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/311314
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/400778
http://e2e.ti.com/support/dlp__mems_micro-electro-mechanical_systems/f/924/t/388917
which indicate the issue I'm having is a known problem with the v2.0 of the firmware, to be fixed in the release of v3.0.
Since v3.0 still hasn't arrived, is it possible that there is a patchedv2.0 that re-enables that feature? I'm happy to use non-guaranteed alpha software if neccessary. Alternatively, is there an archived copy of v1.1 still around (to downgrade but get the feature I need back)? I could not find a download link on the part webpage.
Thanks for any help.
-Zach