This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some questions about DLP 6500 using for design exposure machine

Other Parts Discussed in Thread: DLPC900

hello:

I have some questions. If we want to design exposure machine , we may have a lot of pictures . Through the pattern model to control it. we choose the vedio pattern. I want to ask is this pattern appropriate? Another question i want  to ask so many pictures how to transfer them. The space of flash is not enough.If we want to through vedio pattern,how to set a image to a vedio.

  • Hi,

    Video Pattern can be used when there are many pictures to be displayed.

    You can follow below guidelines  -

    1. Video Timing - Refer to the video timing specification given in the DLPC900 datasheet. Decide what frame-rate you can send the 24-bit pixel data.

    2. Understand how you want the DLPC900 to process in the input 24-bit pixel data. Based on the available time (1/frame-rate) decide which bits and time of exposure of bit(s). Note always make sure the total sum of pattern(s) exposure in 24-bit pixel data is <= 1/frame-rate

    3. Pack the each pattern bit(s) into the 24-bit pixel as per the processing order selected in step #2 above. Once packed you can send the data like any other video frame with timing strictly as per the guidelines in DLPC900 datasheet.

    Regards,

    Sanjeev