This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can't execute DLP LightCrafter 4500 control software...

Other Parts Discussed in Thread: TEST2

Hi sir,

Sir I have installed successfully DLP LightCrafter 4500 control software and firmware....after that device is ready for use..i have created / added BMP images 412X1140 resolution to software. when clicking on   pattern sequence tab there, i added pattern sequence after when i m clicking on send button it  will not successfully execute...image is not appear on device projector..

plz suggest me.  how can execute the device/ software...

  • Hello dipak m,

    The native resolution of the DLP LightCrafter 4500 EVM is 912x1140. In Pattern Sequence Mode, the images must be this resolution to display.

    I am going to move this conversation into our forum dedicated to DLP LightCrafter 4500 topics.

    Best regards,
    Trevor
  • Hello Sir,

    I have done the setting of "Pattern Sequence" in "Operating Mode".


    Today, after getting ur mail. I have everything setting as well as execution also in "Pattern Sequence".which are given below...I m forwarding you everything setting on by pic. also created sample image which are created newly...

    step1- file name ("create image") - created BMP image file resolution 912x1140.. with bit depth 8.

    step2- file name( "added_created_image") -
    firstly added firmware BIN file
    from location where i installed firmware software.
    then after getting default images in added created BMP file. after clicking "save updates" button that saved everything in "test2.bin" file then again I browse "test2.bin" file in firmware file.
    then it shows 11 original images...


    step 3(OPTIONAL)- file name ("video_mode_default_setting.jpg") and
    file name ("video_mode_setting_changed.jpg")
    In both file setting are tested.


    step 4(OPTIONAL)- file name ("periferal_control_Changed_setting.jpg") as well as default settings also tested


    step5-file name ("pattern_sequnce_mode(bit dept=8).jpg") and
    file name ("pattern_sequence_mode(bit dept=1").jpg

    Both setting are tested..




    The Input file you have seen in stpe1.

    The output of these all these settings is Blinking image of default TI image.

    Waiting for u...

    Thanks..
    dipak m