Hi everyone,
I've been browsing to see if any similar questions had been answered but I couldn't find anything. I've been using the Lightcrafter 3000 without the light engine as a hologram for a 660nm laser beam. Everything was working fine yesterday but today when I plugged the device in and connected many of the mirrors were set to random positions and were unresponsive. The splash screen comes up but with a fuzzy back ground due to the frozen mirrors. When I upload a pattern sequence and observe the image a few of the mirrors respond but still, many are set to a random orientation which does not change. Is there any way to reset the mirror positions?
Thanks,
Sam