I am a new user to DLP lightcrafter EVM. I want to use it to trigger a Photron camera FASTCAM-APX RS. But when I use an Oscilloscope to measure the output trigger signal, I found the signal is not TTL but like impulse signal, which was really weird. And the peak amplitude of the signal is very small, less than 1 V, which is useless. I don't know what is wrong. Could the problem be from the connector? And should I make some changes to the circuit? Thank you!