Hi,
I am developing hardware for a research grade confocal microscope. For this purpose, I am using a hacked LightCrafter4500 unit. Illumination and projection hardware are removed, only using the DMD unit for beam steering and shaping.
I understand that there are limits for number of patters stored internally. So, my questions are:
0. I am willing to use 1bit depth patterns.
1. Is there any method to increase number of patterns to about 10,000? Are we limited by the DDR Ram size?
2. I also need fast scanning, less than 100uS per pattern. Any foreseen limitation?
3. If it were possible using external flash, or USB download; would there be any trick to put data (patterns) into the image buffer? Might be slower but would be very convenient and flexible.
I would appreciate your comments and advise a lot.
Regards,
Adnan Kurt