Product Model:DLP® LightCrafter™ Evaluation Module
DMD:0.3 inch WVGA
Question: As figure,the number 1 "Trigger input and output" port,have four pins,now i want use them,but i don't what is the sequence of it,could anyone told me
what line should be linked respectively(from left to the right)?
thanks!
sincerely