Hello:
The 4710 interface is 100pin, can you provide a reference design of the 100pin to the 80pin? As shown in the following picture:
thx for your answers and help.
my Email:fengyang@fengyangtec.com
chang.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Chang,
Hello Chang,
Thank you for your interest in our DLP Technology. This reference design is for the DLP4501 DMD. The DLP4710 DMD chipset contains the DLC3439 controller and DLPA3005.
The DLP4710 DMD can not be used with the DLPC6401. Can you please help me understand what you would like to achieve ?
Best regards,
Nadine
Hello Chang,
I am answering for Nadine today.
I do not understand part of your question.
What is the 4701 and 100pin that you are referring to?
Yes, the DLPC3439 to the DLP4710 interface is through an 80-pin flex cable.
Roger
Hello Chang,
Yes the DLP4710 DMD package has 100 pins.
If you refer to the DLPDLCR4710EVM development platform that uses the DLP4710, you only need an 80 pin connector interface between the DLPC3439s and the DLP4710 DMD.
Please refer to the DLPDLCR4710EVM, http://www.ti.com/lit/pdf/tidrew6 , schematics and the pix below from that schematic.
Regards,
Roger